4.5.3.1 Event Selection

Each counter has an associated control to select one of the event sources. The SELECTn[4:0] bits in HPSEL0 and HPSEL1 select one of the signals that are listed in Table 4-10. The CPU cycle elapsed event is the reference and is incremented on each CPU cycle. The CPU instruction completed event indicates that the CPU pipeline has completed. Comparing instructions completed to cycles elapsed yields the CIP value. The ideal value is one instruction completed per one cycle elapsed. The remaining stall, branch or hazard events can be used to determine where stalls occur and what part of the code to optimize.