24.5.2.3 Receiving Data from a Client Device
The host can receive data from the client device after the host has
transmitted the client address with a R/W status bit value of ‘1’. After receiving an ACK from the client for the address, configure the
packet size (PSZ,(I2CxCON2[15:0]) and then enable the RCEN bit (I2CxCON1[3]) for the first
data byte to be received. If SMART mode SMEN(I2CxCON2 [17]) is enabled, then the hardware
will automatically set RCEN(I2CxCON1[3]) based on the status of RBF(I2CxSTAT1[1]) and
PSZ(I2CxCON2[15:0]) for remaining bytes; otherwise, the user software should set
RCEN(I2CxCON1[3]) for every byte to be received. The host logic begins to generate clocks,
and before each falling edge of the SCLx, the SDAx line is sampled and data are shifted
into the I2CxRSR register.
0’ before attempting to set the RCEN bit. This ensures
that the host logic is inactive.After the falling edge of the eighth SCLx clock, the following events occur:
- The RCEN bit is automatically cleared.
- The contents of the I2CxRSR register transfer into the I2CxRCV register.
- The RBF status bit (I2CxSTAT1[1]) is set.
- The I2C module generates the I2CxIF interrupt if the HDRXIE(I2CxINTC[0]) bit and HSTIE(I2CxINTC[13]) bit are enabled.
When the CPU reads the receive buffer (I2CxRCV), the RBF status bit is automatically cleared. The user software can process the data and then execute an Acknowledge sequence.
If SMART mode is enabled, the hardware will automatically set RCEN(I2CxCON1[3]) based on the status of RBF(I2CxSTAT1[1]) and PSZ(I2CxCON2[15:0]) for the remaining bytes; otherwise the user software should set RCEN(I2CxCON1[3]) for every byte to be received.
If the receive buffer (I2CxRCV) is full and the packet size (I2CxCON2[15:0]) has not reached zero, the I2CxSTAT.SSPND bit is set and the host drives SCL low. The user should remove the Receiver Full condition by reading the receive buffer (I2CxRCV). Once the full condition is removed, I2CxSTAT.SSPND will be cleared by hardware. Once the packet size becomes zero, the end of packet (EOP) will be set (I2CxSTAT2[24]), if enabled (EOPSC, I2CxCON2[20:19]). The sequence of events that occurs during the host reception is illustrated in Figure 24-9.