5.10.1 Execution
main.c - Initialize the chip and retrieve information.
- Code summary:
- Configure the network
parameters in
main.h.
/** Wi-Fi Settings */ #define MAIN_WLAN_SSID "DEMO_AP" /**< Destination SSID */ #define MAIN_WLAN_AUTH M2M_WIFI_SEC_WPA_PSK /**< Security manner */ #define MAIN_WLAN_PSK "12345678" /**< Password for Destination SSID */ - Initialize the socket
module and register the socket callback
function.
/* Initialize socket address structure. */ addr.sin_family = AF_INET; addr.sin_port = _htons(MAIN_WIFI_M2M_SERVER_PORT); addr.sin_addr.s_addr = _htonl(MAIN_WIFI_M2M_SERVER_IP); /* Initialize socket module */ socketInit(); registerSocketCallback(socket_cb, NULL); - Get the MAC address and
set the device name with the MAC address.
m2m_wifi_get_mac_address(gau8MacAddr); set_dev_name_to_mac((uint8_t *)gacDeviceName, gau8MacAddr); set_dev_name_to_mac((uint8_t *)gstrM2MAPConfig.au8SSID, gau8MacAddr); m2m_wifi_set_device_name((uint8_t *)gacDeviceName, ...); - Start the Provision mode.
m2m_wifi_start_provision_mode((tstrM2MAPConfig *)&gstrM2MAPConfig, (char *)gacHttpProvDomainName, 1); - When the mobile device
sends configuration information, the
wifi_cb()function is called with theM2M_WIFI_RESP_PROVISION_INFOmessage and the user can connect to the AP with the given information.static void wifi_cb(uint8_t u8MsgType, void *pvMsg) { case M2M_WIFI_RESP_PROVISION_INFO: tstrM2MProvisionInfo *pstrProvInfo = (tstrM2MProvisionInfo *)pvMsg; if (pstrProvInfo->u8Status == M2M_SUCCESS) { m2m_wifi_connect((char *)pstrProvInfo->au8SSID, strlen((char *)pstrProvInfo->au8SSID), pstrProvInfo->u8SecType, pstrProvInfo->au8Password, M2M_WIFI_CH_ALL); } - After the device is
connected to the AP, the
gethostbyname()function is called.static void wifi_cb(uint8_t u8MsgType, void *pvMsg) { ... case M2M_WIFI_REQ_DHCP_CONF: { ... gbConnectedWifi = true; gethostbyname((uint8_t *)MAIN_WEATHER_SERVER_NAME); } ... } - Create a TCP client
socket and connect to the server in the main loop.
if (gbConnectedWifi && !gbTcpConnection) { if (gbHostIpByName) { if (tcp_client_socket < 0) { if ((tcp_client_socket = socket(AF_INET, SOCK_STREAM, 0)) < 0) { continue; } } if (connect(tcp_client_socket, ...) != SOCK_ERR_NO_ERROR) { continue; } gbTcpConnection = true; } } - The socket callback
function receives the
SOCKET_MSG_CONNECTmessage and then it requests weather information from the server with a city name.static void socket_cb(SOCKET sock, uint8_t u8Msg, void *pvMsg) { case SOCKET_MSG_CONNECT: sprintf(gau8ReceivedBuffer, ..., MAIN_CITY_NAME, ...); ... send(tcp_client_socket, gau8ReceivedBuffer, ...); recv(tcp_client_socket, (struct sockaddr *)&addr_in, sizeof(struct sockaddr_in)); break; } - The socket callback
function receives a
SOCKET_MSG_RECVmessage with weather information. The user can also get the current temperature via an IO1 sensor board as shown in the following.static void socket_cb(SOCKET sock, uint8_t u8Msg, void *pvMsg) { case SOCKET_MSG_RECV: ... /** From the received Josan format buffer City Name, Temperature, Weather Number will be parsed */ /* Get city name. */ pcIndxPtr = strstr((char *)pstrRecv->pu8Buffer, "name="); printf("City: "); ... /* Get temperature. */ pcIndxPtr = strstr(pcEndPtr + 1, "temperature value"); printf("Temperature: "); ... /* Get weather condition. */ pcIndxPtr = strstr(pcEndPtr + 1, "weather number"); if (NULL != pcIndxPtr) { printf("Weather Condition: "); }
- Configure the network
parameters in
main.h.
- Build the program and download it into the board.
- Start the application.
- Connect the mobile device to the ATWINC15x0/ATWINC3400 AP [WINC1500_XX:XX].
- Browse the web page (www.microchip.com) to setup the AP, populate the page and press Connect.
- The ATWINC15x0/ATWINC3400 will be connected to the selected AP.
- The weather information will be printed.
Note: If the server connection is
unstable, this example may not operate normally.