5.3 HTTP File Downloader
This example demonstrates the use of the ATWINC15x0 with the SAM D21 Xplained Pro board to download the file in the SD card connected to the IO1 Xplained Pro board.
Note: This example application is not
            available in ASF for ATWINC3400.
        It is based on the following hardware:
        - The SAM D21 Xplained Pro
 - The ATWINC15x0 on the EXT1 header
 - The IO1 XPRO board on the EXT2 header