3.1 Basic Examples
These examples describe basic Wi-Fi operation in a ‘how-to’ manner:
- How to read the Chip ID (to identify WINC15x0/ATWINC3400 H/W revision differences)
- How to set/get the MAC address of the Wi-Fi module
- How to start Wi-Fi in a specific
operation mode, such as:
- STA Mode (Station mode, known as a Wi-Fi client)
- AP mode (Access Point mode)
- How to switch mode between the STA and AP modes at runtime
- How to scan for nearby APs
- How to set Deep Sleep mode
- How to connect to a secure Wi-Fi network using WEP/WPA/WPA2 security
- How to connect to an enterprise security network
- How to connect via Wi-Fi Protected Setup (WPS)
- How to get an RF signal status by reading the RSSI value
- How to set AP provision using Android App
- How to set HTTP provision