1.6 PCIESS Port List
(Ask a Question)The PCIESS block is generated using the Libero PCIe Configurator. The generation of the PCIESS block includes ports based on the PCIe Configurator settings. The following table lists the port descriptions. The PCIESS also has several status signals, interrupt signals, and power management signals available to the FPGA fabric.
| Port Name | Direction | Description |
|---|---|---|
| AXI_CLK | Input | Global AXI clock. Shared for both PCIESS interfaces. |
| AXI_CLK_STABLE | Input | Clock lock signal. Indicates that the AXI_CLK source from the fabric is locked and ready for use. |
| Master | ||
| PCIESS_AXI_#_M_ARADDR[31:0] | Output | Read address. The address of the first transfer in a read burst transaction. |
| PCIESS_AXI_#_M_ARBURST[1:0] | Output | Read burst type. The burst type and the size details determine how the address for each transfer within the burst is calculated. |
| PCIESS_AXI_#_M_ARID[3:0] | Output | Read address ID. Identification tag for the read address group of signals. |
| PCIESS_AXI_#_M_ARLEN[7:0] | Output | Burst length. Indicates the exact number of transfers in a burst. |
| PCIESS_AXI_#_M_ARREADY | Input | Read address ready. Indicates that the slave is ready to accept an address and associated control signals. |
| PCIESS_AXI_#_M_ARSIZE[2:0] | Output | Burst size. Indicates the size of each transfer in the burst. |
| PCIESS_AXI_#_M_ARVALID | Output | Read address valid. Indicates that the channel is signaling valid read address and control information. |
| PCIESS_AXI_#_M_AWADDR[31:0] | Output | Write address. The address of the first transfer in a write burst transaction. |
| PCIESS_AXI_#_M_AWBURST[1:0] | Output | Write burst type. The burst type and the size of information determine how the address for each transfer within the burst is calculated. |
| PCIESS_AXI_#_M_AWID[3:0] | Output | Write address ID. Identification tag for the write address group of signals. |
| PCIESS_AXI_#_M_AWLEN[7:0] | Output | Burst length. Indicates the exact number of transfers in a burst, which determines the number of data transfers associated with the address. |
| PCIESS_AXI_#_M_AWREADY | Input | Write address ready. Indicates that the slave is ready to accept an address and associated control signals. |
| PCIESS_AXI_#_M_AWSIZE[2:0] | Output | Burst size. Indicates the size of each transfer in the burst. |
| PCIESS_AXI_#_M_AWVALID | Output | Write address valid. Indicates that the channel is signaling valid write address and control information. |
| PCIESS_AXI_#_M_BID[3:0] | Input | Response ID tag. Identification tag for the write response. |
| PCIESS_AXI_#_M_BREADY | Output | Response ready. Indicates that the master is ready to accept a write response. |
| PCIESS_AXI_#_M_BRESP[1:0] | Input | Write response. Indicates the status of the write transaction. When it is asserted to 2'b10 (SLVERR/DECERR), unsupported request to PCIe is reported. |
| PCIESS_AXI_#_M_BVALID | Input | Write response valid. Indicates that the channel is signaling a valid write response. |
| PCIESS_AXI_#_M_RDATA[63:0] | Input | Read data. |
| PCIESS_AXI_#_M_RID[3:0] | Input | Read ID tag. Identification tag for the read data group of signals generated by the slave. |
| PCIESS_AXI_#_M_RLAST | Input | Read last. Indicates the last transfer in a read burst. |
| PCIESS_AXI_#_M_RREADY | Output | Read ready. Indicates that the master can accept the read data and associated control signals, along with response information. |
| PCIESS_AXI_#_M_RRESP[1:0] | Input | Read response. Indicates the status of the read transfer.
|
| PCIESS_AXI_#_M_RVALID | Input | Read valid. Indicates that the channel is signaling the required read data. |
| PCIESS_AXI_#_M_WDATA[63:0] | Output | Write data. |
| PCIESS_AXI_#_M_WLAST | Output | Write last. Indicates the last transfer in a write burst. |
| PCIESS_AXI_#_M_WREADY | Input | Write ready. Indicates that the slave can accept the write data. |
| PCIESS_AXI_#_M_WSTRB[7:0] | Output | Write strobes. Indicates the byte lanes that hold valid data. There is one write strobe bit for every eight bits of the write data bus. |
| PCIESS_AXI_#_M_WVALID | Output | Write valid. Indicates that valid write data and strobes are available. |
| Slave | ||
| PCIESS_AXI_#_S_ARADDR[31:0] | Input | Read address. The address of the first transfer in a read burst transaction. |
| PCIESS_AXI_#_S_ARBURST[1:0] | Input | Burst type. The burst type and the size of information determine how the address for each transfer within the burst is calculated. |
| PCIESS_AXI_#_S_ARID[3:0] | Input | Read address ID. Identification tag for the read address group of signals. |
| PCIESS_AXI_#_S_ARLEN[7:0] | Input | Burst length. Indicates the exact number of transfers in a burst. |
| PCIESS_AXI_#_S_ARREADY | Output | Write address ready. Indicates that the slave is ready to accept an address and the associated control signals. |
| PCIESS_AXI_#_S_ARSIZE[2:0] | Input | Burst size. Indicates the size of each transfer in the burst. |
| PCIESS_AXI_#_S_ARVALID | Input | Read address valid. Indicates that the channel is signaling valid read address and control information. |
| PCIESS_AXI_#_S_AWADDR[31:0] | Input | Write address. Address of the first transfer in a write burst transaction. |
| PCIESS_AXI_#_S_AWBURST[1:0] | Input | Burst type. The burst type and the size information determine how the address for each transfer within the burst is calculated. |
| PCIESS_AXI_#_S_AWID[3:0] | Input | Write address ID. Identification tag for the write address group of signals. |
| PCIESS_AXI_#_S_AWLEN[7:0] | Input | Burst length. Indicates the exact number of transfers in a burst, which determines the number of data transfers associated with the address. |
| PCIESS_AXI_#_S_AWREADY | Output | Write address ready. Indicates that the slave is ready to accept an address and associated control signals. |
| PCIESS_AXI_#_S_AWSIZE[2:0] | Input | Burst size. Indicates the size of each transfer in the burst. |
| PCIESS_AXI_#_S_AWVALID | Input | Write address valid. Indicates that the channel is signaling valid write address and control information. |
| PCIESS_AXI_#_S_BID[3:0] | Output | Response ID tag. Identification tag for the write response. |
| PCIESS_AXI_#_S_BREADY | Input | Response ready. Indicates that the master can accept a write response. |
| PCIESS_AXI_#_S_BRESP[1:0] | Output | Write response. Indicates the status of the write transaction. It is asserted to 2'b10(SLVERR), when:
|
| PCIESS_AXI_#_S_BVALID | Output | Write response valid. Indicates that the channel is signaling a valid write response. |
| PCIESS_AXI_#_S_RDATA[63:0] | Output | Read data. |
| PCIESS_AXI_#_S_RID[3:0] | Output | Read ID tag. Identification tag for the read data group of signals generated by the slave. |
| PCIESS_AXI_#_S_RLAST | Output | Read last. Indicates the last transfer in a read burst. |
| PCIESS_AXI_#_S_RREADY | Input | Read ready. Indicates that the master can accept the read data and response information. |
| PCIESS_AXI_#_S_RRESP[1:0] | Output | Read response. Indicates the status of the read transfer. It is asserted to 2'b10(SLVERR), when:
|
| PCIESS_AXI_#_S_RVALID | Output | Read valid. Indicates that the channel is signaling the required read data. |
| PCIESS_AXI_#_S_WDATA[63:0] | Input | Write data. |
| PCIESS_AXI_#_S_WLAST | Input | Write last. Indicates the last transfer in a write burst. |
| PCIESS_AXI_#_S_WREADY | Output | Write ready. Indicates that the slave can accept the write data. |
| PCIESS_AXI_#_S_WSTRB[7:0] | Input | Write strobes. Indicates the byte lanes that hold valid data. There is one write strobe bit for each eight bits of the write data bus. |
| PCIESS_AXI_#_S_WVALID | Input | Write valid. Indicates that valid write data and strobes are available. |
| PCIe | ||
| PCIE_#_M_RDERR | Input | Tie to 0 |
| PCIE_#_M_WDERR | Output | Not connected |
| PCIE_#_S_RDERR | Output | Not connected |
| PCIE_#_S_WDERR | Input | Tie to 0 |
| PCIE_#_HOT_RST_EXIT | Output | Hot reset exit. Asserted for one clock cycle when the LTSSM exits Hot Reset state. Prompts the application layer to perform a global reset. |
| PCIE_#_DLUP_EXIT | Output | DL-up exit. Indicates transition from DL_UP to DL_DOWN.
|
| PCIE_#_INTERUPT[7:0] | Input | Local interrupt input ports. The fabric logic can drive up to eight interrupt sources by generating a pulse (high) on the ports and the clock pluses are asserted. [7:0] can be used for MSI. [0] is also available for INTx. Used only for endpoints. PCIESS uses TL_CLK to monitor this signal. MSI offsets are [negotiated interrupt-1:negotiated interrupt-8] |
| PCIE_#_INTERUPT_OUT | Output | Local interrupt output port. Indicates that one of the possible interrupt sources was detected and the user can read the interrupt through the DRI. It is a level sensitive signal; whenever an interrupt described in ISTATUS_LOCAL, SEC_ERROR_INT register, DED_ERROR_INT register, and PCIE_EVENT_INT register is active, the PCIE_#_INTERUPT_OUT signal gets asserted and remains high. It is low when the corresponding interrupts in the registers are cleared. |
| PCIE_#_LTSSM[4:0] | Output | LTSSM state encoding: 0x0: LTSSM_DET_QUIET 0x1: LTSSM_DET_ACT 0x2: LTSSM_POL_ACT 0x3: LTSSM_POL_COMP 0x4: LTSSM_POL_CFG 0x5: LTSSM_CFG_LWSTR 0x6: LTSSM_CFG_LWACC 0x7: LTSSM_CFG_LWAIT 0x8: LTSSM_CFG_LNACC 0x9: LTSSM_CFG_CPLT 0xa: LTSSM_CFG_IDLE 0xb: LTSSM_RCV_RLOCK 0xc: LTSSM_RCV_EQL 0xd: LTSSM_RCV_SPEED 0xe: LTSSM_RCV_RCFG 0xf: LTSSM_RCV_IDLE 0x10: LTSSM_L0 0x11: LTSSM_L0S 0x12: LTSSM_L1_ENTRY 0x13: LTSSM_L1_IDLE 0x14: Reserved 0x15: Reserved 0x16: LTSSM_DISABLED 0x17: LTSSM_LOOPBACK_ENTRY 0x18: LTSSM_LOOPBACK_ACTIVE 0x19: LTSSM_LOOPBACK_EXIT 0x1a: LTSSM_HOTRESET |
| PCIE_#_PERST_N | Input | Asynchronous. PERST_N can use any GPIO. |
| PCIE_#_TL_CLK_125MHz | Input | 125 MHz (maximum) clock input. Continuous running clock is required for PCIe core transaction layer. Connects to the DIV_CLK output from the TX_PLL. TL_CLK is available only after PCIe initialization. User have to derive from the on-chip oscillator to drive the TL_CLK during PCIe initialization. An NGMUX can be used to switch this clock to the required DIV_CLK after PCIe initialization. For information about PolarFire FPGA reference design, see PolarFire FPGA PCIe EndPoint DDR3L DDR4 Memory Controller Data Plane. For information about PolarFire SoC FPGA Linux reference design, see GitHub. |
| Transceiver | ||
| CLKS_FROM_TXPLL_TO_PCIE_# | Input | PCIE_#_TX_BIT_CLK_#: This port must be driven by the BIT_CLK output of the Tx PLL. Gen1 2.5 G, Gen2 5 G, and mix of Gen 1 and Gen 2 is 2.5 G. |
| PCIE_#_TX_PLL_REF_CLK_#: Reference clock from TX_PLL. | ||
| PCIE_#_TX_PLL_LOCK_#: Lock status input to PCIESS. Connects to the lock output of the TX_PLL. | ||
| PCIESS_LANE#_CDR_REF_CLK_# | Input | Reference clock to lane CDR. Connects to the REF_CLK input of the TX_PLL. |
| PCIESS_LANE_TXDn_P | Output | Transceiver differential output transmit data. n = 0, 1, 2, 3. |
| PCIESS_LANE_TXDn_N | ||
| PCIESS_LANE_RXDn_P | Output | Transceiver differential input receive data. n = 0, 1, 2, 3. |
| PCIESS_LANE_RXDn_N | ||
|
Note:
| ||