47.2 Extended Instruction Set
In addition to the standard instruction set, PIC18 devices also provide an optional extension to the core CPU functionality. The added features include additional instructions that augment Indirect and Indexed Addressing operations and the implementation of Indexed Literal Offset Addressing mode for many of the standard PIC18 instructions.
The additional features of the extended instruction set are disabled by default. To enable them, users must set the XINST Configuration bit.
The instructions in the extended set can all be classified as literal
			operations, which either manipulate the File Select registers or use them for Indexed
			Addressing. Two of the standard instructions, ADDFSR and
				SUBFSR, each have an additional special instantiation for using
			FSR2 as extended instructions. These versions (ADDULNK and
				SUBULNK) allow for automatic return after execution.
The extended instructions are specifically implemented to optimize re-entrant program code (that is, code that is recursive or that uses a software stack) written in high-level languages, particularly C. Among other things, they allow users working in high-level languages to perform certain operations on data structures more efficiently. These include:
- Dynamic allocation and deallocation of software stack space when entering and leaving subroutines
 - Function pointer invocation
 - Software Stack Pointer manipulation
 - Manipulation of variables located in a software stack
 
A summary of the instructions in the extended instruction set is provided in Extended Instruction Syntax. Detailed descriptions are provided in Extended Instruction Set. The opcode field descriptions in Table 47-1 apply to both the standard and extended PIC18 instruction sets.
- The instruction set extension and the Indexed Literal Offset Addressing mode were designed for optimizing applications written in C; the user may likely never use these instructions directly in assembler. The syntax for these commands is provided as a reference for users who may be reviewing code that has been generated by a compiler.
 - Enabling the PIC18 instruction set extension may cause legacy applications to behave erratically or fail entirely. Refer to Byte-Oriented and Bit-Oriented Instructions in Indexed Literal Offset Mode for details.