1.1.7.4.20 DRV_SDSPI_EVENT Enum
C
typedef enum
{
/* Operation has been completed successfully. */
DRV_SDSPI_EVENT_COMMAND_COMPLETE = SYS_MEDIA_EVENT_BLOCK_COMMAND_COMPLETE,
/* There was an error during the operation */
DRV_SDSPI_EVENT_COMMAND_ERROR = SYS_MEDIA_EVENT_BLOCK_COMMAND_ERROR
} DRV_SDSPI_EVENT;
Summary
Identifies the possible events that can result from a request.
Description
This enumeration identifies the possible events that can result from a read or a write request issued by the client.
Remarks
One of these values is passed in the "event" parameter of the event handling callback function that client registered with the driver by calling the DRV_SDSPI_EventHandlerSet function when a request is completed.
Remarks
Refer sys_media.h for definition of SYS_MEDIA_XXX.