1.1.7.4.8 DRV_SDSPI_SyncWrite Function
C
bool DRV_SDSPI_SyncWrite(
const DRV_HANDLE handle,
void* sourceBuffer,
uint32_t blockStart,
uint32_t nBlock
)Summary
Writes blocks of data starting at the specified address of the SD Card.
Description
This function performs a blocking write operation to write blocks of data to the SD Card. The function returns true if the request was successfully executed. The function returns false under the following circumstances:
- if the driver handle is invalid
- if the source buffer pointer is NULL
- if the number of blocks to be written is either zero or more than the number of blocks actually available
- if the SD card is write-protected
- if there was an error during the SD card write operation
Precondition
The DRV_SDSPI_Initialize routine must have been called for the specified SDSPI driver instance.
DRV_SDSPI_Open routine must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open function |
| sourceBuffer | The source buffer containing data to be written to the SD Card. |
| blockStart | Starting block address of SD Card where the writes should begin. |
| nBlock | Total number of blocks to be written. |
Returns
true - If the request was executed successfully.
false - If there was an error executing the request.
Example
#define MY_BUFFER_SIZE 1024 uint8_t CACHE_ALIGN myBuffer[MY_BUFFER_SIZE]; // Address must be block aligned. uint32_t blockStart = 0x00; uint32_t nBlock = 2; // mySDSPIHandle is the handle returned by the DRV_SDSPI_Open function. if (DRV_SDSPI_SyncWrite(mySDSPIHandle, myBuffer, blockStart, nBlock) == true) { // Write is successful } else { // Error handling here }
Remarks
None.