1.1.7.4.6 DRV_SDSPI_SyncRead Function
C
bool DRV_SDSPI_SyncRead (
const DRV_HANDLE handle,
void* targetBuffer,
uint32_t blockStart,
uint32_t nBlock
)Summary
Reads blocks of data from the specified block address of the SD Card.
Description
This function performs a blocking read operation to read blocks of data from the SD Card. The function returns true if the request was successfully executed; returns false otherwise. The function returns false under following conditions:
- if the driver handle is invalid
- if the target buffer pointer is NULL
- if the number of blocks to be read is zero or more than the actual number of blocks available.
- Error during the read operation
Precondition
The DRV_SDSPI_Initialize routine must have been called for the specified SDSPI driver instance.
DRV_SDSPI_Open must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open function |
| targetBuffer | Buffer into which the data read from the SD Card will be placed |
| blockStart | Starting block address of the SD Card from where the read should begin. |
| nBlock | Total number of blocks to be read. |
Returns
true - If the request was executed successfully.
false - If there was an error executing the request.
Example
#define MY_BUFFER_SIZE 1024 uint8_t CACHE_ALIGN myBuffer[MY_BUFFER_SIZE]; // Address must be block aligned. uint32_t blockStart = 0x00; uint32_t nBlock = 2; // mySDSPIHandle is the handle returned by the DRV_SDSPI_Open function. if (DRV_SDSPI_SyncRead(mySDSPIHandle, myBuffer, blockStart, nBlock) == true) { // Read successful } else { // Error handling here }
Remarks
None.