1.1.7.4.5 DRV_SDSPI_Tasks Function
C
void DRV_SDSPI_Tasks
(
SYS_MODULE_OBJ object
)Summary
Maintains the driver's state machine.
Description
This routine is used to maintain the driver's internal state machine. For synchronous driver, the task routine periodically checks for SD card attach/detach event and initializes the SD card.
Precondition
The DRV_SDSPI_Initialize routine must have been called for the specified SDSPI driver instance.
Parameters
| Param | Description |
|---|---|
| object | Object handle for the specified driver instance (returned from DRV_SDSPI_Initialize) |
Returns
None
Example
//sysObj.drvSDSPI0 is returned by the driver initialization routine //For synchronous driver while(1) { DRV_SDSPI_Tasks(sysObj.drvSDSPI0); // Yield and allow other threads to run vTaskDelay(100 / portTICK_PERIOD_MS); }
Remarks
This routine is normally not called directly by an application.
For synchronous driver with RTOS, this routine is called from a separate RTOS thread.