1.1.7.4.12 DRV_SDSPI_GeometryGet Function
C
SYS_MEDIA_GEOMETRY* DRV_SDSPI_GeometryGet
(
const DRV_HANDLE handle
)Summary
Returns the geometry of the device.
Description
This API gives the following geometrical details of the SD Card.
- Media Property
- Number of Read/Write/Erase regions in the SD Card
- Number of Blocks and their size in each region of the device
Precondition
The DRV_SDSPI_Initialize routine must have been called for the specified SDSPI driver instance.
The DRV_SDSPI_Open routine must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open function |
Returns
SYS_MEDIA_GEOMETRY - Pointer to structure which holds the media geometry information.
Example
SYS_MEDIA_GEOMETRY * SDSPIGeometry; uint32_t readBlockSize, writeBlockSize, eraseBlockSize; uint32_t nReadBlocks, nReadRegions, totalSize; // mySDSPIHandle is the handle returned by the DRV_SDSPI_Open function. SDSPIGeometry = DRV_SDSPI_GeometryGet(mySDSPIHandle); readBlockSize = SDSPIGeometry->geometryTable->blockSize; nReadBlocks = SDSPIGeometry->geometryTable->numBlocks; nReadRegions = SDSPIGeometry->numReadRegions; writeBlockSize = (SDSPIGeometry->geometryTable +1)->blockSize; eraseBlockSize = (SDSPIGeometry->geometryTable +2)->blockSize; totalSize = readBlockSize * nReadBlocks * nReadRegions;
Remarks
Refer sys_media.h for definition of SYS_MEDIA_GEOMETRY.