1.1.7.4.2 DRV_SDSPI_Status Function
C
SYS_STATUS DRV_SDSPI_Status
(
SYS_MODULE_OBJ object
)Summary
Provides the current status of the SDSPI driver module.
Description
This routine provides the current status of the SDSPI driver module.
Precondition
Function DRV_SDSPI_Initialize must have been called before calling this function
Parameters
| Param | Description |
|---|---|
| object | Driver object handle, returned from the DRV_SDSPI_Initialize routine |
Returns
SYS_STATUS_READY - Indicates that the driver has been initialized and is ready to accept requests from the client.
SYS_STATUS_UNINITIALIZED - Indicates that the driver has not been initialized.
Example
SYS_MODULE_OBJ object; // Returned from DRV_SDSPI_Initialize
SYS_STATUS status;
status = DRV_SDSPI_Status(object);
if (status == SYS_STATUS_READY)
{
// Driver is initialized and ready.
}Remarks
This operation can be used to determine if the driver is initialized or not.