1.1.4.4.1 DRV_NAND_FLASH_Initialize Function

C

SYS_MODULE_OBJ DRV_NAND_FLASH_Initialize
(
    const SYS_MODULE_INDEX drvIndex,
    const SYS_MODULE_INIT *const init
)

Summary

Initializes the NAND Flash Driver.

Description

This routine initializes the NAND Flash driver making it ready for client to use.

  • Get the data address of NAND Flash

Precondition

None.

Parameters

ParametersDescription
drvIndexIdentifier for the instance to be initialized
initPointer to a data structure containing any data necessary to initialize the driver

Returns

If successful, returns a valid handle to a driver instance object. Otherwise, it returns SYS_MODULE_OBJ_INVALID.

Example

// This code snippet shows an example of initializing the NAND FLASH Driver
// with NAND FLASH device attached.

SYS_MODULE_OBJ objectHandle;

const DRV_NAND_FLASH_PLIB_INTERFACE drvNandFlashPlibAPI = {
    .DataAddressGet = SMC_DataAddressGet,
    .CommandWrite = SMC_CommandWrite,
    .CommandWrite16 = SMC_CommandWrite16,
    .AddressWrite = SMC_AddressWrite,
    .AddressWrite16 = SMC_AddressWrite16,
    .DataWrite = SMC_DataWrite,
    .DataWrite16 = SMC_DataWrite16,
    .DataRead = SMC_DataRead,
    .DataRead16 = SMC_DataRead16,
    .DataPhaseStart = PMECC_DataPhaseStart,
    .StatusIsBusy = PMECC_StatusIsBusy,
    .ErrorGet = PMECC_ErrorGet,
    .RemainderGet = PMECC_RemainderGet,
    .ECCGet = PMECC_ECCGet,
    .ErrorLocationGet = PMERRLOC_ErrorLocationGet,
    .ErrorLocationDisable = PMERRLOC_ErrorLocationDisable,
    .SigmaSet = PMERRLOC_SigmaSet,
    .ErrorLocationFindNumOfRoots = PMERRLOC_ErrorLocationFindNumOfRoots
};

const DRV_NAND_FLASH_INIT drvNandFlashInitData =
{
    .nandFlashPlib = &drvNandFlashPlibAPI,
};

objectHandle = DRV_NAND_FLASH_Initialize((SYS_MODULE_INDEX)DRV_NAND_FLASH_INDEX, (SYS_MODULE_INIT *)&drvNandFlashInitData);

if (SYS_MODULE_OBJ_INVALID == objectHandle)
{
    // Handle error
}

Remarks

This routine must be called before any other NAND Flash driver routine is called.

This routine should only be called once during system initialization.