1.1.4.4.16 DRV_NAND_FLASH_SkipBlock_BlockWrite Function

C

bool DRV_NAND_FLASH_SkipBlock_BlockWrite(const DRV_HANDLE handle, uint16_t blockNum, uint8_t *data, bool disableBlockCheck)

Summary

Writes the data of a whole block to NAND Flash.

Description

This function schedules a blocking operation for writing the data of a whole block to NAND Flash.

Precondition

The DRV_NAND_FLASH_Open() routine must have been called for the specified NAND Flash driver instance.

Parameters

ParametersDescription
handleA valid open-instance handle, returned from the driver's open routine
blockNumBlock number to write
dataPointer to source data buffer
disableBlockCheck

0 - Block will be checked as good before writing a given block

1 - Block will not check before writing a given block

Returns

True - If Block write is successfully completed.

False - If Block write fails.

Example

DRV_HANDLE handle; // Returned from DRV_NAND_FLASH_Open
uint16_t blockNum = 3;
static uint8_t blockBuffer[262144 + 14336];

memset(blockBuffer, 0x55, sizeof(blockBuffer));

if (DRV_NAND_FLASH_SkipBlock_BlockWrite(handle, blockNum, blockBuffer, 0))
{
    // Block write successfully completed
}

Remarks

This routine will block wait until write request is submitted successfully. Client should wait until write is complete to send next transfer request.