1.1.4.4.7 DRV_NAND_FLASH_IdRead Function
C
bool DRV_NAND_FLASH_IdRead(const DRV_HANDLE handle, uint32_t *readId, uint8_t address)Summary
Gets identifier codes from NAND Flash.
Description
This routine read identifier codes from NAND Flash.
Preconditions
The DRV_NAND_FLASH_Open() routine must have been called for the specified NAND Flash driver instance.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| readId | Pointer to 32-bit unsigned int into which ID will be stored |
| address | Address to be send after command cycle. Address 0x20 is used for ONFI compliant Flash. |
Returns
True - If ID read successfully from the Flash.
False - If invalid handle.
Example
#define NAND_FLASH_ADDR_ONFI_SIGNATURE 0x20
uint32_t readId = 0;
DRV_HANDLE handle; // Returned from DRV_NAND_FLASH_Open
if (DRV_NAND_FLASH_IdRead(handle, &readId, NAND_FLASH_ADDR_ONFI_SIGNATURE))
{
// ID read successfully
}Remarks
This routine will block for hardware access.