1.1.4.4.14 DRV_NAND_FLASH_SkipBlock_BlockErase Function
C
bool DRV_NAND_FLASH_SkipBlock_BlockErase(const DRV_HANDLE handle, uint16_t blockNum, bool disableBlockCheck)Summary
Erase a block.
Description
This function schedules a blocking block erase operation of Flash memory. It erases a given block.
Preconditions
The DRV_NAND_FLASH_Open() routine must have been called for the specified NAND Flash driver instance.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| blockNum | Block number to be erased |
| disableBlockCheck |
0 - Block will be checked as good before erasing a given block 1 - Block will not check before erasing a given block |
Returns
True - If the block erase is successfully completed.
False - If block erase fails.
Example
uint16_t blockNum = 0; DRV_HANDLE handle; // Returned from DRV_NAND_FLASH_Open if(DRV_NAND_FLASH_SkipBlock_BlockErase(handle, blockNum, 0)) { // Block erase is successfully completed }
Remarks
This routine will block wait until erase request is completed successfully. Client should wait until erase is complete to send next transfer request.