1.1.4.4.10 DRV_NAND_FLASH_GeometryGet Function
C
bool DRV_NAND_FLASH_GeometryGet( const DRV_HANDLE handle, DRV_NAND_FLASH_GEOMETRY *geometry );Summary
Returns the geometry of the NAND Flash device.
Description
This API gives the following geometrical details of the NAND Flash:
deviceId (JEDEC Manufacturer ID)
Bus Width
Number of data bytes per page
Number of spare bytes per page
Block Size
Device Size
Number of logical units
Number of bits of ECC correction
Precondition
The DRV_NAND_FLASH_Open() routine must have been called for the specified NAND Flash driver instance.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| geometry | Pointer to destination geometry buffer into which geometry to be placed |
Returns
True - If geometry is successfully read from the NAND Flash.
False - If geometry read is failed.
Example
DRV_HANDLE handle; // Returned from DRV_NAND_FLASH_Open
DRV_NAND_FLASH_GEOMETRY nandFlashFlashGeometry;
if (DRV_NAND_FLASH_GeometryGet(handle, &nandFlashFlashGeometry))
{
// Geometry read successfully
}Remarks
This routine will block wait for hardware access.