1.1.3.4.20 DRV_MEMORY_AddressGet Function

C

uintptr_t DRV_MEMORY_AddressGet
(
    const DRV_HANDLE handle
);

Summary

Returns the Memory media start address.

Description

This function returns the Memory Media start address.

Precondition

The DRV_MEMORY_Open() routine must have been called to obtain a valid opened device handle.

Parameters

ParametersDescription
handleA valid open-instance handle, returned from the driver's open function

Returns

Start address of the Memory Media if the handle is valid, otherwise NULL.

Example

uintptr_t startAddress;
startAddress = DRV_MEMORY_AddressGet(drvMEMORYHandle);

Remarks

None.