1.1.3.4.5 DRV_MEMORY_Close Function
C
void DRV_MEMORY_Close( const DRV_HANDLE handle );Summary
Closes an opened-instance of the Memory driver.
Description
This routine closes an opened-instance of the Memory driver, invalidating the handle.
After calling this routine, the handle passed in "handle" must not be used with any of the remaining driver routines. A new handle must be obtained by calling DRV_MEMORY_Open before the caller may use the driver again. Usually there is no need for the driver client to verify that the Close operation has completed.
Precondition
DRV_MEMORY_Open must have been called to obtain a valid opened device handle.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
Returns
None.
Example
DRV_HANDLE handle; // Returned from DRV_MEMORY_Open DRV_MEMORY_Close(handle);
Remarks
None.