1.1.3.4.15 DRV_MEMORY_TransferStatusGet Function

C

MEMORY_DEVICE_TRANSFER_STATUS DRV_MEMORY_TransferStatusGet
(
    const DRV_HANDLE handle
);

Summary

Gets the current status of the transfer request on attached device.

Description

This routine gets the current status of the transfer request. The application must use this routine where the status of a scheduled request needs to be polled on.

The application can alternatively register a transfer handler to receive the transfer completion events.

Precondition

DRV_MEMORY_Open() must have been called to obtain a valid opened device handle.

Parameters

ParametersDescription
handleA valid open-instance handle, returned from the driver's open function

Returns

  • MEMORY_DEVICE_TRANSFER_ERROR_UNKNOWN

    • If the handle is invalid
    • If the status read request fails
  • MEMORY_DEVICE_TRANSFER_BUSY

    • If the current transfer request is still being processed
  • MEMORY_DEVICE_TRANSFER_COMPLETED

    • If the transfer request is completed

Example

// memoryHandle is the handle returned by the DRV_MEMORY_Open function.

if (MEMORY_DEVICE_TRANSFER_COMPLETED == DRV_MEMORY_TransferStatusGet(memoryHandle))
{
    // Operation Done
}

Remarks

This routine will block for hardware access. Used in Async mode of operation.