1.1.3.4.19 DRV_MEMORY_IsWriteProtected Function

C

bool DRV_MEMORY_IsWriteProtected
(
    const DRV_HANDLE handle
);

Summary

Returns the write-protect status of the Memory.

Description

This function returns the write-protect status of the Memory.

Precondition

The DRV_MEMORY_Open() routine must have been called to obtain a valid opened device handle.

Parameters

ParametersDescription
handleA valid open-instance handle, returned from the driver's open function

Returns

True - If the memory is write-protected.

False - If the memory is not write-protected.

Example

bool isWriteProtected;

isWriteProtected = DRV_MEMORY_IsWriteProtected(drvMEMORYHandle);

Remarks

None.