1.1.3.4.11 DRV_MEMORY_SyncWrite Function

C

bool DRV_MEMORY_SyncWrite
(
    const DRV_HANDLE handle,
    void *sourceBuffer,
    uint32_t blockStart,
    uint32_t nBlock
);

Summary

Writes data for the specified number of memory blocks in Synchronous mode.

Description

This function schedules a blocking write operation for writing blocks of data into attached devices memory.

Precondition

DRV_MEMORY_Open() routine must have been called to obtain a valid opened device handle. The memory block which has to be written, must have been erased before using the DRV_MEMORY_xxxErase() routine.

Parameters

ParametersDescription
handleA valid open-instance handle, returned from the driver's open function
sourceBufferThe source buffer containing data to be programmed into media device memory
blockStartBlock start from where the data should be written to
nBlockTotal number of blocks to be written

Returns

  • True:

    • If the transfer request is successfully completed
  • False:

    • If the source buffer pointer is NULL
    • If the client opened the driver for read-only
    • If the number of blocks to be written is either zero or more than the number of blocks actually available
    • If the driver handle is invalid

Example

#define BUFFER_SIZE 4096
uint8_t writeBuffer[BUFFER_SIZE];

// Use DRV_MEMORY_GeometryGet () to find the write region geometry.
uint32_t blockStart = 0x0;
uint32_t nBlock = BUFFER_SIZE / block_size; // block_size for write geometry

// memoryHandle is the handle returned by the DRV_MEMORY_Open function.

if(DRV_MEMORY_SyncErase(memoryHandle, blockStart, nBlock) == false)
{
    // Error handling here
}

if(DRV_MEMORY_SyncWrite(memoryHandle, &writeBuffer, blockStart, nBlock) == false)
{
    // Error handling here
}

Remarks

This API is supported only in RTOS environment.