1.1.3.4.7 DRV_MEMORY_SyncErase Function

C

bool DRV_MEMORY_SyncErase
(
    const DRV_HANDLE handle,
    uint32_t blockStart,
    uint32_t nBlock
);

Summary

Erase the specified number of memory blocks in Synchronous mode.

Description

This function schedules a blocking sector erase operation for the specified number of memory blocks from the specified block start address on attached memory device.

Precondition

The DRV_MEMORY_Open() must have been called with DRV_IO_INTENT_WRITE or DRV_IO_INTENT_READWRITE as a parameter to obtain a valid opened device handle.

Parameters

ParametersDescription
handleA valid open-instance handle, returned from the driver's open function
blockStartblock start from where the blocks should be erased
nBlockTotal number of blocks to be erased

Returns

  • True:

    • If the transfer request is successfully completed
  • False:

    • If the client opened the driver for read-only
    • If the number of blocks to be erased is either zero or more than the number of blocks actually available
    • If the driver handle is invalid

Example

// Use DRV_MEMORY_GeometryGet () to find the erase region geometry.
uint32_t blockStart = 0;
uint32_t nBlocks = 10;

// memoryHandle is the handle returned by the DRV_MEMORY_Open function.

if(DRV_MEMORY_SyncErase( memoryHandle, blockStart, nBlock ) == false)
{
    // Error handling here
}

Remarks

This API is supported only in RTOS environment.