1.1.3.4.12 DRV_MEMORY_AsyncRead Function

C

void DRV_MEMORY_AsyncRead
(
    const DRV_HANDLE handle,
    DRV_MEMORY_COMMAND_HANDLE *commandHandle,
    void *targetBuffer,
    uint32_t blockStart,
    uint32_t nBlock
);

Summary

Reads data for the specified number of memory blocks in Asynchronous mode.

Description

This function schedules a non-blocking read operation for reading blocks of data from the memory device attached.

The function returns with a valid command handle in the commandHandle argument if the request was scheduled successfully.

The function adds the request to the hardware instance queue and returns immediately. While the request is in the queue, the application buffer is owned by the driver and should not be modified.

The function returns DRV_MEMORY_COMMAND_HANDLE_INVALID in the commandHandle argument under the following circumstances:

  • if a buffer object could not be allocated to the request
  • if the target buffer pointer is NULL
  • if the client opened the driver for write-only
  • if the number of blocks to be read is either zero or more than the number of blocks actually available
  • if the driver handle is invalid

Precondition

DRV_MEMORY_Open() must have been called with DRV_IO_INTENT_READ or DRV_IO_INTENT_READWRITE as the ioIntent to obtain a valid opened device handle.

Parameters

ParametersDescription
handleA valid open-instance handle, returned from the driver's open function
commandHandlePointer to an argument that will contain the command handle
targetBufferBuffer into which the data read from the media device memory will be placed
blockStartBlock start from where the data should be read
nBlockTotal number of blocks to be read

Returns

The command handle is returned in the commandHandle argument. It will be DRV_MEMORY_COMMAND_HANDLE_INVALID if the request was not successful.

Example

uint8_t readBuffer[BUFFER_SIZE];

// Use DRV_MEMORY_GeometryGet () to find the read region geometry.
// Find the block address from which to read data.
uint32_t blockStart = 0x0;
uint32_t nBlock = BUFFER_SIZE;
DRV_MEMORY_COMMAND_HANDLE commandHandle;
bool xfer_done = false;

// memoryHandle is the handle returned by the DRV_MEMORY_Open function.

// Event is received when the read request is completed.
void appTransferHandler
(
    DRV_MEMORY_EVENT event,
    DRV_MEMORY_COMMAND_HANDLE commandHandle,
    uintptr_t context
)
{
    switch(event)
    {
        case DRV_MEMORY_EVENT_COMMAND_COMPLETE:
        {
            xfer_done = true;
            break;
        }

        case DRV_MEMORY_EVENT_COMMAND_ERROR:
        {
            // Handle Error
            break;
        }

        default:
        {
            break;
        }
    }
}

DRV_MEMORY_TransferHandlerSet(memoryHandle, appTransferHandler, (uintptr_t)NULL);

DRV_MEMORY_AsyncRead(memoryHandle, &commandHandle, &readBuffer, blockStart, nBlock);

if(DRV_MEMORY_COMMAND_HANDLE_INVALID == commandHandle)
{
    // Error handling here
}

while(!xfer_done);

Remarks

This API is supported in Both Bare-Metal and RTOS environment.