1.1.3.4.2 DRV_MEMORY_Status Function

C

SYS_STATUS DRV_MEMORY_Status( SYS_MODULE_OBJ object );

Summary

Gets the current status of the Memory driver module.

Description

This routine provides the current status of the Memory driver module.

Precondition

Function DRV_MEMORY_Initialize should have been called before calling this function.

Parameters

ParametersDescription
objectDriver object handle, returned from the DRV_MEMORY_Initialize routine

Returns

SYS_STATUS_READY - Indicates that the driver is ready and accept requests for new operations.

SYS_STATUS_UNINITIALIZED - Indicates the driver is not initialized.

SYS_STATUS_BUSY - Indicates the driver is in busy state.

Example

SYS_MODULE_OBJ object; // Returned from DRV_MEMORY_Initialize
SYS_STATUS MEMORYStatus;

MEMORYStatus = DRV_MEMORY_Status(object);

Remarks

This routine will never block waiting for hardware.