4.9.2 Enable/Disable Wi-Fi/BT Co-existence support
To configure Wi-Fi®/Bluetooth® coexistence
(Wi-Fi/Bluetooth co-ex) PTA settings, use the WILC
sysfs nodes in Linux
root file-system (rootFS). These sysfs entries are created when the WILCS02 driver is loaded successfully. There are four
sysfs configuration entries to setup the Wi-Fi/Bluetooth co-ex PTA
settings. These configurations file nodes can be listed using ls
command.Note: PTA configuration entries are in
bold.# ls /sys/wilc/
ant_swtch_mode coex_enabled fw_dbg_mod_filter
antenna1 coex_inteface_type p2p_mode
antenna2 coex_wlan_bt_priority
coex_antenna_mode fw_dbg_level
The following table contains more details on these sysfs nodes and their
default values when they are created.
| Node | Value |
|---|---|
coex_antenna_mode |
|
coex_inteface_type |
|
coex_wlan_bt_priority |
|
coex_enabled |
|
- To read the values of the
Wi-Fi/Bluetooth co-ex, use the following
catcommand:# cat /sys/wilc/coex_antenna_mode 0 # cat /sys/wilc/coex_inteface_type 0 # cat /sys/wilc/coex_wlan_bt_priority 3 # cat /sys/wilc/coex_enabled 1
-
To modify the values of the Wi-Fi/Bluetooth co-ex, use the following
echocommand:# echo <value> > /sys/wilc/coex_antenna_mode # echo <value> > /sys/wilc/coex_wlan_bt_priority # echo <value> > /sys/wilc/coex_inteface_type # echo <value> > /sys/wilc/coex_enabled
The Wi-Fi/Bluetooth PTA default configurations are applied during the WLAN host driver/firmware initialization. To change the PTA configurations, modify the configurations once the network interface (wlan0) is up.
Note:
- Changing the
configuration parameters (for example,
coex_antenna_mode,coex_wlan_bt_priorityand more) does not take effect while the Wi-Fi/Bluetooth co-ex is running. The recommendation is to change these parameters before enabling the Wi-Fi/Bluetooth co-ex by using thecoex_enabledcommand. - To turn OFF Bluetooth
operation while the Wi-Fi/Bluetooth co-ex is enabled, perform the
following steps:
- Use the following command to disable the Wi-Fi/Bluetooth co-ex
feature:
echo <value> > /sys/wilc/coex_enabled -
When turning the Bluetooth operation back ON, the Bluetooth must be turned ON first. This is to avoid leaving the PTA pins floating when the Bluetooth operation is OFF without enabling the Wi-Fi/Bluetooth co-ex.
- Use the following command to disable the Wi-Fi/Bluetooth co-ex
feature: