VDDIO2 is available as an internal input channel to the ADC. The
voltage is divided by 10 to allow the use of any internal ADC reference. To measure
VDDIO2, follow these steps:
Configure the voltage reference for the
ADC
Select VDDIO2 as the positive
input to the ADC
Run a single-ended ADC conversion
Calculate the voltage using the following
equation: