The Virtual PORT registers map the most frequently used regular PORT registers
into the I/O Register space with single-cycle bit access.
Access to
the Virtual PORT registers has the same outcome as access to the regular registers but
allows for memory specific instructions, such as bit manipulation instructions, which
cannot be used in the extended I/O Register space where the regular PORT registers
reside.
The following table shows the
mapping between the PORT and VPORT registers.
Table 1. Virtual Port Mapping
Regular PORT Register |
Mapped to Virtual PORT Register |
PORTx.DIR |
VPORTx.DIR |
PORTx.OUT |
VPORTx.OUT |
PORTx.IN |
VPORTx.IN |
PORTx.INTFLAGS |
VPORTx.INTFLAGS |
Note: Avoid accessing the mapped VPORT register using the single-cycle I/O instructions
immediately after accessing the regular PORT register. This may cause a memory collision
since the single-cycle I/O access to VPORT is faster than the regular PORT register access.