Generating the IAP Update Design

This section describes the steps to create IAP update design for the IAP Target by executing the TCL script available in the design files. In this design, the SPI Flash client is generated with the IAP image. This image is used for IAP. Before you start, ensure that the version of IP cores in the Libero SoC vault is exactly the same as specified in <$download_directory>\mpf_an4568_v2022p1_df\TARGET_C\common.tcl.

Follow these steps:

  1. 1.Ensure that the hardware is setup as described in Setting Up the Hardware.
  2. 2.On the host PC, launch Libero SoC.
  3. 3.Select Project > Execute Script.
  4. 4.Select Browse and select script.tcl from <$download_directory>\mpf_an4568_v2022p1_df\TARGET_C\script.tcl.
  5. 5.Select Run. After successful execution of the TCL script, the Libero SoC project for IAP update is created (iap_target_c.prjx).
Tip: For more information about TCL commands, see Libero® SoC TCL Command Reference Guide. Contact Microchip Support for any queries about running the TCL script.