Installing the GUI

Follow these to install the GUI:
  1. 1.Extract the mpf_an4568_v2022p1_df.zip file.
  2. 2.Double click the setup.exe file from <$download_directory>\mpf_an4568_v2022p1_df\GUI.
  3. 3.Follow the instructions on the installation wizard. After successful installation, the SmartSFP demo appears on the start menu of the host PC.

This concludes installing the demo. See Running the Demo for running the demo.