16.4.2.2 Slope Generation Mode
The slope generator function can be utilized in Peak Current-mode
control-based power supply applications, where slope compensation is required. The slope
function modifies the non-slope PDM DAC value repeatedly, at a user-defined rate, until
the DAC data value reaches its endpoint. The slope generation function can be enabled or
disabled by the SLOPEN bit (SLPxCON[31]). The slope rate is controlled by the data in
the SLPxDAT register. The direction of slope being positive or negative is controlled by
the PSE bit (SLPxCON[25]). For negative slopes (default, PSE = 0), DACDAT holds the nominal non-slope count, while DACLOW holds the count
corresponding to the end of the slope. For positive slopes (PSE = 1), DACLOW holds the nominal non-slope count, while DACDAT
holds the count corresponding to the end of the slope.
The slope generation start is controlled by the bits, SLPSTRT[3:0] (SLPxCON[3:0]). Depending on the value of SLPSTRT[3:0], the selected PWM trigger will be used to start the slope generation. The DAC output voltage changes to the value in DACDAT first by going to the Transition mode and then to the Steady-State mode. In Transition mode, the filter responds to new data values as fast as possible. The Transition mode duration is specified by the TMODTIME[9:0] bits (DACCTRL2[9:0]). The Transition mode duration, TTR, is given by the equation:
TTR = TMODTIME[9:0] * 2/FDAC in Seconds
Where: FDAC = DAC Frequency in Hz
The steady-state timer, specified by the SSTIME[9:0] bits, starts at the same time as the Transition mode timer. Once the Transition mode ends, the Steady-State mode starts, wherein the DAC output voltage settles to the new value. The Steady-State Time, TSS, is calculated by the equation:
TSS = SSTIME[9:0] * 2/FDAC in Seconds
Note that the SSTIME[9:0] count should always be greater than the TMODTIME[9:0] count. At the end of the Steady-State mode, the DAC value settles at the new value and is ready for slope generation. The SLPSTRT[3:0] signal triggers the slope generation process.
Refer to the DAC electrical specifications for additional information on TSS and TTR values. These timing parameters can be additionally adjusted as needed for the application.
The slope generation is terminated when one of the two stop signals is asserted. The eight control register bits, SLPSTOPA[3:0] (SLPxCON[11:8]) and SLPSTOPB[3:0] (SLPxCON[7:4]), select the control signal to terminate the slope generation. The stop signals are logically ORed so that the slope is terminated when one of the trigger events materializes. In most power supply applications, SLPSTOPA[3:0] can be configured to terminate the slope at the end of the PWM cycle, while SLPSTOPB[3:0] can be configured to trigger when the current reaches a limit under a normal or Fault condition. It should be noted that the stop signal must terminate the slope at least TSS (Steady-State Time) prior to the next PWM cycle start. This is necessary to allow the DAC value to reach and settle at the steady-state value, specified by DACDAT, before the next cycle begins.
The slope rate value to be specified in the SLPxDAT register depends on the start and end values of the slope specified by DACDAT and DACLOW, PWM time period, DAC clock frequency and the SSTIME[9:0] bits value. The SLPxDAT value can be determined by using the below equation.
Where:
DACDAT = DAC value at the start of slope
DACLOW = DAC value and the end of slope
TSLOPE_DURATION = Slope duration time in seconds
TDAC = 2/FDAC in seconds