40.13.5 Pipe Status Register n
Name: | PSTATUSn |
Offset: | 0x0106 + n*0x20 [n=0..7] |
Reset: | 0x00 |
Property: | PAC Write-Protection |
Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
BK1RDY | BK0RDY | PFREEZE | CURBK | DTGL | |||||
Access | R | R | R | R | R | ||||
Reset | 0 | 0 | 0 | 0 | 0 |
Bit 7 – BK1RDY Bank 1 is ready
Writing a one to the bit EPSTATUSCLR.BK1RDY will clear this bit.
Writing a one to the bit EPSTATUSSET.BK1RDY will set this bit.
This bank is not used for Control pipe.
Value | Description |
---|---|
0 | The bank number 1 is not ready: For IN the bank is empty. For Control/OUT the bank is not yet fill in. |
1 | The bank number 1 is ready: For IN the bank is filled full. For Control/OUT the bank is filled in. |
Bit 6 – BK0RDY Bank 0 is ready
Writing a one to the bit EPSTATUSCLR.BK0RDY will clear this bit.
Writing a one to the bit EPSTATUSSET.BK0RDY will set this bit.
This bank is the only one used for Control pipe.
Value | Description |
---|---|
0 | The bank number 0 is not ready: For IN the bank is not empty. For Control/OUT the bank is not yet fill in. |
1 | The bank number 0 is ready: For IN the bank is filled full. For Control/OUT the bank is filled in. |
Bit 4 – PFREEZE Pipe Freeze
Writing a one to the bit EPSTATUSCLR.PFREEZE will clear this bit.
Writing a one to the bit EPSTATUSSET.PFREEZE will set this bit.
- When a STALL handshake has been received.
- After a PIPE has been enabled (rising of bit PEN.N).
- When an LPM transaction has completed whatever handshake is returned or the transaction was timed-out.
- When a pipe transfer was completed with a pipe error. See the PINTFLAG register.
When PFREEZE bit is set while a transaction is in progress on the USB bus, this transaction will be properly completed. PFREEZE bit will be read as “1” only when the ongoing transaction will have been completed.
Value | Description |
---|---|
0 | The Pipe operates in normal operation. |
1 | The Pipe is frozen and no additional requests will be sent to the device on this pipe address. |
Bit 2 – CURBK Current Bank
Value | Description |
---|---|
0 | The bank0 is the bank that will be used in the next single/multi USB packet. |
1 | The bank1 is the bank that will be used in the next single/multi USB packet. |
Bit 0 – DTGL Data Toggle Sequence
Writing a one to the bit EPSTATUSCLR.DTGL will clear this bit.
Writing a one to the bit EPSTATUSSET.DTGL will set this bit.
This bit is toggled automatically by hardware after a data transaction.
This bit will reflect the data toggle in regards of the token type (IN/OUT/SETUP).
Value | Description |
---|---|
0 | The PID of the next expected transaction will be zero: data 0. |
1 | The PID of the next expected transaction will be one: data 1. |