7.5.16 Customer Configurable Command
Description
The SPI command “Customer Configurable Command” is used to extend the SPI command set by the customer as follows:
“Customer Configurable Command” calls the function that is stored in customCmd.customPtr which points to an address in the Flash or user ROM. This command is not available in the ATA8215.
Command Frame
| Host |
0x14 |
0x00 |
| ATA8210/15 |
events.system |
events.events |
Parameters
- 0x14 – Command ID
- 0x00 – Dummy byte (no information)
Return Values
- events.system – Event byte (for details see SPI command “Get Event Bytes”)
- events.events – Event byte (for details see SPI command “Get Event Bytes”)