7.5.12 Patch SPI
Description
The SPI command “Patch SPI” is used to extend the SPI command set by the customer as follows:
Patch_Spi (uint8_t parameter) jumps to the function which is stored in extif.flashPtr. The parameter of Patch_Spi is located in the SPDR register. The Patch SPI extension has no return and the customer has to finish with a jump to PATCH_SPI_READY (which is the same as SPIBUFRDY_DISABLERXBUFINT).
Command Frame
| Host |
0x0F |
parameter |
| ATA8210/15 |
events.system |
events.events |
Parameters
- 0x0F – Command ID
- Parameter – One possible parameter for the patch SPI function (located in SPDR register)
Return Values
- events.system – Event byte (for details see SPI command “Get Event Bytes”)
- events.events – Event byte (for details see SPI command “Get Event Bytes”)