4.4.3.2.1.5 DMCRA – Demodulator Control Register for Path A
This register must only be modified if the block receiving the settings is disabled (RDPR.PRPTA = 1). Modifying the settings during operation may lead to unstable operation.
| Name: | DMCRA |
| Offset: | 0x0A6 |
| Reset: | 0x00 |
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
| DMARA | SY1TA | SASKA | DMPGA[4:0] | ||||||
| Access | R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W | |
| Reset | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |
Bit 7 – DMARA Demodulator Automatic Restart on Path A
| Bit 7 | Description |
|---|---|
0 | The reception and demodulation is continued regardless of error events. |
1 | Reception and demodulation are restarted if any activated condition for the EOTA interrupt is true. The EOTA condition status flags (EOTS[3:0]) and the SOTA condition status flags (SOTSA) are cleared at every restart. The restart is automatically performed by toggling the RDPR.PRPTA bit. The PRPTA bit is not writable while the automatic mode is active. |
Bit 6 – SY1TA Symbol Check with 1T Only on Path A
| Bit 6 | Description |
|---|---|
0 | The symbol timing check accepts HIGH and LOW times with the selected symbol period (1T) and the double symbol period (2T). Random Manchester data can be used as the preamble in this mode. |
1 | The symbol timing check allows HIGH and LOW times with the selected symbol rate only. This corresponds to an alternating preamble of 1 and 0 symbols. It is a more rigorous criterion and, therefore, leads to shorter average on-times. The 1T check is performed for the number of bits specified in the SYCSA register. Afterward, 1T and 2T are acceptable (corresponding to random Manchester). |
Bit 5 – SASKA Select ASK Input for Path A
| Bit 5 | Description |
|---|---|
0 | FSK input is selected for receiving path A |
1 | ASK input is selected for receiving path A |
Bits 4:0 – DMPGA[4:0] FSK Demodulator PLL Loop Gain for Path A
Calculation of the target PLL loop gain for the maximum symbol rate
- Equation parameters:
- SymbolRatePathA: Maximum expected symbol rate in Hz on the useful signal for path A
- CLK_BB: Baseband clock frequency in Hz. See equation (13) in Bandwidth Scaling. See Bandwidth Scaling in the Channel Filter from Related Links.
- Equation parameters:
- DeviationPathA is the maximum expected frequency deviation in Hz of the useful signal for path A
- CLK_BB is the baseband clock frequency in Hz. See equation (13) in Bandwidth Scaling. See Bandwidth Scaling in the Channel Filter from Related Links.
- Selection of the required PLL loop gain, which is the larger one of the two gains
- Selection of the DMPGA value according to the required PLL loop gain
- The PLL_GAIN_A must be selected from the following table to be greater than or equal to the REQ_PLL_GAIN.
- If REQ_PLL_GAIN ≥ 1, set DMPGA = 16. The corresponding DMPGA value is the correct setting for this register.
| PLL_GAIN_A | DMPGA(Dec) |
|---|---|
| 0.06 | 0 |
| 0.08 | 1 |
| 0.09 | 2 |
| 0.11 | 3 |
| 0.13 | 4 |
| 0.16 | 5 |
| 0.19 | 6 |
| 0.22 | 7 |
| 0.25 | 8 |
| 0.31 | 9 |
| 0.38 | 10 |
| 0.44 | 11 |
| 0.50 | 12 |
| 0.63 | 13 |
| 0.75 | 14 |
| 0.88 | 15 |
| ≥ 1.00 | 16 |