3.9.8 mcUtils_LinearRamp
C
/* Linear ramp function */
void mcUtils_LinearRamp(int32_t * const input, const int32_t stepSize, const int32_t finalValue)
Summary
This function performs the linear ramp on a given input value.
Description
This function adjusts an input value incrementally towards a final value using a specified step size. This function is typically used to implement a linear ramp for control applications, ensuring a smooth transition between values.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| input | Pointer to the current value that will be adjusted towards the final value. |
| stepSize | The incremental step size used to adjust the input value. |
| finalValue | The target value that the input value is adjusted towards. |
Returns
None
Example
int32_t currentValue=0; /* Call the linear ramp function in a loop or control function */ mcUtils_LinearRamp(¤tValue, 1, 10);
Remarks
None.