3.9.4 mcUtils_PiIntegralUpdate
C
/* Updates the integral part of the floating point PI control */ void mcUtils_PiIntegralUpdate( const float32_t value, tmcUtils_PiControl_s * const pControl ) /* Updates the integral part of the fixed point PI control */ void mcUtils_PiIntegralUpdate(const int16_t value, tmcUtils_PiControl_s * const pControl)
Summary
Updates the integral part of the PI control.
Description
This function updates the integral term of the PI control with the specified value.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| value | Integral value to be updated. Please refer the generated header for the exact data type. |
| pControl | Pointer to the PI control structure to be updated. |
Returns
None
Example
/ Define the PI control module data structure tmcUtils_PiControl_s piControl; // Define the parameters for floating point PI control float32_t Ki_value = 1.0f; // Define the parameters for fixed point PI control int16_t Ki_value = 1; mcUtils_PiControlInit(Ki_value, &piControl);
Remarks
Refer the generated header file for the exact function signature.