3.9.5 mcUtils_PiControlReset
C
/* Resets the floating point PI control output. */ void mcUtils_PiControlReset(const float32_t integral, tmcUtils_PiControl_s * const pControl) /* Resets the fixed point PI control output. */ void mcUtils_PiControlReset(const int32_t out, tmcUtils_PiControl_s * const pControl)
Summary
Resets the output of the PI control.
Description
This function resets the PI controller by setting the integral output to the specified values.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| integral | The output value to be reset. Please refer the generated header for the exact data type. |
| pControl | Pointer to the PI control structure that holds the controller's state and parameters. |
Returns
None
Example
// Define the PI controller data structure tmcUtils_PiControl_s piControl; // Define the parameters for floating point PI control float32_t value = 0.0f; // Define the parameters for fixed point PI control int32_t value = 0; /* Resets the PI control output */ mcUtils_PiControlReset(value, &piControl);
Remarks
Refer the generated header file for the exact function signature..