3.9.6 mcUtils_PiControlInit
C
/* Initializes the PI control structure with the given parameters. */
void mcUtils_PiControlInit( float32_t Kp, float32_t Ki, float32_t dt,
tmcUtils_PiControl_s * const pControl)
Summary
Initializes the PI control structure with the given parameters.
Description
The function initializes the PI controller by setting its proportional gain
(Kp) and calculating the effective integral gain
(Ki). The integral gain is scaled by the sampling time
(dt) to accommodate discrete-time integration.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| Kp | Proportional gain of the PI controller. |
| Ki | Integral gain of the PI controller |
| dt | Sampling time |
| pControl | Pointer to the PI control structure that needs to be initialized. |
Returns
None
Example
tmcUtils_PiControl_s piControl; float32_t Kp = 1.0f; float32_t Ki = 0.5f; float32_t dt = 0.0001f; mcUtils_PiControlInit(Kp, Ki, dt, &piControl);
Remarks
None.