3.11.10 Q15_ANGLE Macro
C
#define Q15_ANGLE(value) (int16_t)( value * (float32_t)Q15_SCALE_FACTOR / (float32_t)ONE_PI)
Summary
Convert the given value into an angle represented in the Q15 fixed-point format.
Description
The macro converts a given value into an angle represented in the Q15 fixed-point
format. It achieves this by scaling the input value using a predefined scaling
factor, Q15_SCALE_FACTOR(), and then normalizing it by dividing by π.
Example
float32_t angle_value = 3.14f;
int16_t result = Q15_ANGLE(angle_value); // Converts the value into a Q15 angle
Remarks
None