3.28.9 FRER Configuration
Use this command to configure Frame Replication and Elimination for Reliability (FRER) parameters.
Command Syntax:
tsn frer <inst>
mode { generation | recovery }
admin-state { enable | disable }
frer-vlan <vid>
recovery algorithm { match | vector [ history-length <history_len> ] }
recovery reset-timeout <reset_timeout>
recovery take-no-sequence
recovery individual
recovery terminate
recovery latent-error-detection [ difference <diff> ] [ period <period> ] [ paths <paths> ] [ resetperiod <reset_period> ]
ingress stream-id-list <stream_list>
egress interface <port_type> [ <port_list> ]Argument | Description | |
Parameter |
| FRER instance number. The valid range is 1–127. |
| FRER VLAN ID | |
| The valid range is 2–32 and the default value is 2. | |
| Reset timeout in milliseconds. The valid range is 1–4095 and default is 1000. | |
| The valid range is 0–10000000 and the default value is 100. | |
| The valid range is 1000–86400000 and the default value is 2000. | |
| The valid range is 2–4 and the default value is 2. | |
| The valid range is 1000–86400000 and the default value is 30000. | |
| Maximum limit of 8 ingress streams | |
| Port type in GigabitEthernet | |
| List of Port ID, for example, 1/1,3-5. | |
Default | N.A | |
Mode | Global Configuration mode and TSN FRER Configuration mode | |
Usage | Configure FRER parameters | |
Example | Example 1: | |