3.28.5 TAS SDU Configuration
Use this command to configure the Maximum SDU size parameter for the traffic class supported by the port.
Command Syntax:
tsn tas max-sdu queue <queue> <sdu>Argument | Description | |
Parameter |
| Specific queue or range from 0–7. |
| Integer in the range 0–10240. The default value is 1536. | |
Default | N.A | |
Mode | Port List Interface mode | |
Usage | Configure TAS SDU size for the port. | |
Example | Example 1: | |