1.2.5.66 SPW_PKTTX_SetNextSendList

void SPW_PKTTX_SetNextSendList(uint8_t* routerBytesTable,
                               SPW_PKTTX_SEND_LIST_ENTRY* sendListAddress,
                               uint16_t length,
                               bool abort,
                               SPW_PKTTX_NXTSEND_START startMode,
                               uint8_t startValue)

Summary

Set the SPW next send list informations and start conditions

Preconditions

None

Parameters

  • routerBytesTable - Table of 4 router bytes to prepend (if non-zero) to each packets in the send list. All bytes are set to 0 if this pointer is NULL

  • sendListAddress - Pointer to the send list type object that will be transmitted

  • length - Number of entries in send list

  • abort - Set to True if any ongoing send list should be abort when this send list wants to start

  • startMode - Send list start mode condition

  • startValue - Matching value for event start condition

Returns

None