3.1 Board Feature Location
The development board layout is shown in the following figure.
The following table provides the details and descriptions of the development board features.
| Number | Description of Item |
|---|---|
| 1 | Micro-USB Type-AB Host/Device DRD |
| 2 | MCU Current Measurement Jumper |
| 3 | User Switch 0 |
| 4 | User Switch 1 |
| 5 | Micro-USB Type-AB from PKOB4 |
| 6 | Extension Power Header |
| 7 | Cortex® 10-pin Debug Interface |
| 8 | EXT1 Header |
| 9 | USERLDO Header |
| 10 | CryptoAuthentication device, TA101 |
| 11 | EXT2 Header |
| 12 | RTC Header |
| 13 | 10 kOhms Potentiometer |
| 14 | CAN1 Interface Header |
| 15 | CAN2 Interface Header |
| 16 | Touch Button |
| 17 | Arduino UNO R3 Shield Headers |
| 18 | 3.3V High-Precision Voltage Reference (bottom side) |
| 19 | PIC32CM SG00/GC00 Microcontroller |
| 20 | mikroBUS Headers |
| 21 | Reset Switch |
| 22 | User LED0/LED1 |