14. Module: QEI
|
When the QEI is configured with Position Counter Initialization Mode bits (PIMOD[2:0]) equal to 0b001, 0b010, 0b011, 0b100 or 0b111, any index event initializes the position counter. However, if the clock divider value configured by the INTDIV[2:0] bits is greater than 1, and if the index event occurs between two clock edges, the index event will be missed. | |||||||||||||||||
| Work around The index pulse width should be sufficiently high enough so that the event is captured by the QEI clock. | |||||||||||||||||
Affected Silicon Revisions
|