1.4.3.17 PAL_Status Function
C
SYS_STATUS PAL_Status(SYS_MODULE_OBJ object);
Summary
Gets the current status of the PAL module.
Description
This routine provides the current status of the PAL module.
Precondition
The PAL_Initialize function should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| object | Identifier for the object instance |
Returns
SYS_STATUS_READY: Indicates that the driver is ready and accept requests for new operations.
SYS_STATUS_UNINITIALIZED: Indicates the driver is not initialized.
SYS_STATUS_ERROR: Indicates the driver is not initialized correctly.
SYS_STATUS_BUSY: Indicates the driver is initializing.
Example
SYS_MODULE_OBJ sysObjPal;
sysObjPal = PAL_Initialize(PRIME_PAL_INDEX);
SYS_STATUS status;
status = PAL_Status(sysObjPal);
Remarks
None