1.4.3.37 PAL_CheckMinimumQuality Function
C
bool PAL_CheckMinimumQuality(uint16_t pch, uint8_t reference, uint8_t modulation);
Summary
Check minimum quality for modulation scheme
Description
This routine is used to check if the modulation is good enough for a low FER (Frame Error rate) for the given scheme.
Precondition
The PAL_Initialize function should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| pch | Physical channel |
| scheme | Modulation scheme of message |
| lessRobustMode | Less robust modulation |
Returns
true - If successful
false - If unsuccessful
Example
uint16_t pch = 16;
PAL_SCHEME scheme = PAL_PLC_DBPSK_R;
uint8_t lessRobustMode = PAL_PLC_DQPSK;
bool result=true;
result = PAL_HasMinimumQuality(pch, scheme, lessRobustMode);
Remarks
Not available for PHY Serial.