1.4.3.30 PAL_GetChannel Function
C
uint8_t PAL_GetChannel(uint16_t *pPch, uint16_t channelReference);
Summary
Get the band (PLC) or the pch (RF).
Description
This routine is used to get the pch or band used for the communication.
Precondition
The PAL_Initialize function should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| pch | Physical channel |
| channelReference | Physical channel in the same channels range |
Returns
PAL_CFG_SUCCESS - If successful
PAL_CFG_INVALID_INPUT - If unsuccessful
Example
uint8_t result=PAL_CFG_SUCCESS;
uint16_t pPch=0;
uint16_t channelRef=1;
result = PAL_GetChannel(&pch, channelRef);
Remarks
Not available for PHY Serial.