1.4.3.28 PAL_SetAGC Function
C
uint8_t PAL_SetAGC(uint16_t pch, uint8_t mode, uint8_t gain);
Summary
Set the automatic gain mode of the PHY PLC layer.
Description
This routine is used to set Automatic Gain Mode (AGC) of the PHY PLC layer.
Precondition
The PAL_Initialize function should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| pch | Physical channel |
| mode | Auto/Manual mode (auto mode(0), manual mode(1)) |
| gain | Initial receiving gain in auto mode |
Returns
PAL_CFG_SUCCESS - If successful
PAL_CFG_INVALID_INPUT - If unsuccessful
Example
uint8_t result=PAL_CFG_SUCCESS;
uint8_t mode=0;
uint8_t gain=0;
uint16_t pch=1;
result = PAL_SetAGC(pch, mode, gain);
Remarks
Not available for PHY Serial and PHY RF.